AXIS#.WS.CHECKT

Description

This parameter sets the amount of time a commutation error must be present before a fault occurs. Commutation monitoring is disabled when this parameter is set to 0.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

ms

Range

0 to 10,000

Default Value

10
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
AXIS1.WS.CHECKT

5013h

10h

Unsigned16

-

-

Read/Write

No

AXIS2.WS.CHECKT

5113h

10h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.WS.CHECKT

6715

1A3B

Unsigned16

Read/Write

-

AXIS2.WS.CHECKT

72251

11A3

Unsigned16

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.WS.CHECKT

6715

Unsigned16

Read/Write

-